Insights Hub How to enable Software Tab under Device on IoT Extension

2021-06-18T19:12:31Z
Connectivity

Summary


Details

You have successfully onboarded a device to IoT Extension in MindSphere and now you want to enable the software tab to update or downgrade the firmware on a device. By default, this tab is not enabled when a device is onboarded using MQTT.


Solution

When a device is being onboarded to IoT Extension you will need to send the "114" MQTT template with a list of supported operations. To enable the software tab simply add the "c8y_SoftwareList" to the "114" template.

Example message:

"114,c8y_SoftwareList"

Notes

KB Article ID# PL8551943

Contents

SummaryDetails

Associated Components

MindConnect IoT Extension