A Solid Edge license file may have a special name such as, for example, "SELicense - 2021-06-11T095832.795.dat" or "ugslmd_NodeLocked_09-Mar-2021 (1).lic".
Can such a license file be renamed by a user without causing problems running the software?
Solution
A license file does not change its internal structure when renaming it or giving it a new file extension.
The file extension will only provide the information that is required for the program to run on a computer once you double click on it in File Manager. The name itself of a License file is not relevant for Solid Edge.
The recommendation is to give the file the extension ".lic" because this makes identifying a license easier.
The license file itself is simply a Text file that can be edited and modified with editors such as Notepad or Wordpad.
NotesIf you have further inquiries about Node Locked Licensing please refer to the FAQs collection link below: