Timeseries 400 Bad request while executing PUT on the IoT Timeseries API

2021-07-16T12:34:19Z

Summary


Details

When you are trying to insert/update the data by using a PUT request with the IoT Timeseries API, you get a error as shown below:

Sample BODY :

[

    {

        "test_variable1": 23.16,

        "test_variable2": 4.0711,

        "test_variable3": 76.8542,

        "test_variable4": 42.0224,

        "test_variable5": 50.0655,

        "test_variable6": 7.0664,

        "test_variable8": 12.6881,

        "_time": "2021-06-14T08:40:02.881118100Z"

    }

]

{

    "timestamp": "2021-06-14T08:59:41.415+00:00",

    "status": 400,

    "error": "Bad Request",

    "message": "[6404] One or more invalid property names specified. One invalid property - test_variable8",

    "path": "/api/iottimeseries/v3/timeseries/617b5d378def40d2865f2ad99c57512f/Test_Aspect"

}

Solution

This error comes when you are trying to insert the data by using PUT API to the variable(test_variable) which doesn't exist for the given aspect. To verify this you need to hit GET API and need to check if the variable exists in the list or not.

GET:

https://gateway.eu1.mindsphere.io/api/iottimeseries/v3/timeseries/Test_Aspect

Sample Response:

[

    {

        "test_variable1": 15.16,

        "test_variable2": 4.0711,

        "test_variable3": 76.8542,

        "test_variable4": 42.0224,

        "test_variable5": 25.0655,

        "test_variable6": 7.0664,

        "test_variable7": 12.6881,

        "_time": "2021-06-14T08:50:02.881118100Z"

    }

]

Here you can see that "test_variable8" doesn't exist in the response, so you can not update the data with respect to "test_variable8".

If the variable does not belong to the list, then you have to define a correct variable in the payload and send a PUT request to the API.

Notes

KB Article ID# PL8551118

Contents

SummaryDetails

Associated Components