Changing the Revision Rule used when opening Solid Edge files.

2021-10-06T23:58:40Z

Summary


Details

How do you change the Revision Rule used when opening an assembly in Solid Edge? 



Solution

On the File Open dialog there is a group of Panes along the right side of the dialog. Select the Open Options pane (the icon is of a folder with a green gear in the bottom right corner) to access the Revision Rule selection. Using the dropdown, select the desired revision Rule.


If the Open Options pane is not displaying on the right side of the File Open dialog turn it, on with the Panes command in the middle of the toolbar at the top of the screen. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 001-10086481

KB Article ID# PL8550402

Contents

SummaryDetails

Associated Components