You want to connect a Raspberry Pi to Insights Hub.
SolutionInsights Hub offers plenty of options to connect the tiny and popular Raspberry Pi computer.
In conjunction with our Start for Free offering, we have tutorials for onboarding a Raspberry Pi device:
https://documentation.mindsphere.io/resources/html/start-for-free/en-US/136504183435.html
Using our flexible MindConnect IoT Extension:
https://developer.mindsphere.io/howto/howto-rpi-mciot.html
The following are not specific to the Raspberry Pi, but more general connectivity and work well on the device.
If you already have an existing solution, you can always incorporate the MindConnect API:
https://developer.mindsphere.io/apis/connectivity-mindconnect/api-mindconnect-overview.html
Haven't found a solution that works for you? You have the option to build a custom agent using popular SDKs including Java, Node.js, Python and more. Visit our developer site for details and examples: https://developer.mindsphere.io
Our Insights Hub community is also a great resource to connect with Raspberry Pi enthusiasts and see what is possible: https://community.sw.siemens.com/s/topic/0TO4O000000MihsWAC/insights-hub
Notes
Notes