NX The behavior of automatic entering in sketcher task in hole command

2021-10-06T23:28:00Z
NX for Design

Summary


Details

From NX1953 onwards, when you select the face as the hole position, it does not automatically enter the sketcher task environment.

Solution

Prior to NX1953, when you select the face as the hole position, it used to automatically enter the sketcher task environment.

But from NX1953 onwards, the behavior has been enhanced in the hole command.
Now a point will be created at the selected location and the respective positioning dimensions are displayed in the graphics window when the user selects the face as the Hole position.
User can directly edit these dimensions without the need to enter the Sketcher application.


If the user still wants to modify the positioning in sketcher, he can select the Sketcher icon in the dialog to enter the application as before.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1953
Function: FEATURE_MODEL

Ref: 002-8549665

KB Article ID# PL8549665

Contents

SummaryDetails

Associated Components

Modeling