NX Additive Manufacturing Replaces Minus Sign or Blank Space in the file name with an underscore

2021-10-06T23:27:59Z
NX for Manufacturing

Summary


Details

A part with a Minus Sign "-" or a Blank Space " " in the file name is sent through the Materialize NX Additive Manufacturing build processor. The process replaces these characters in the output file name with an underscore "_". Is there a way to generate the output file without changing the file name?

Solution

The Materialize build processor cannot accept file names containing a space or minus sign. This is why these characters are converted to an underscores before outputting the data to the processor. This is a known limitation. There is no workaround for this. 

Notes and References


Hardware/Software Configuration

Platform: all
OS: n-a
OS Version: n-a
Product: NX
Application: CAM
Version: V1973
Function: ADDITIVE

Ref: 001-10076049

KB Article ID# PL8548995

Contents

SummaryDetails

Associated Components

Manufacturing Additive