Tecnomatix Controllers for YASKAWA_INFORM

2024-07-17T06:17:40Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "YASKAWA_INFORM"
are available for download from https://support.sw.siemens.com.

See Tecnomatix__changes_log.html for details concerning this update.
Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select Tecnomatix 16.1, 16.1.1, 16.1.2, 17.0, 2206, 2301, 2307 or 2402
-Select Tecnomatix 16.1 Robot Controllers, Tecnomatix 16.1.1 Robot Controllers, Tecnomatix 16.1.2 Robot Controllers, Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers, Tecnomatix 2301 Robot Controllers, Tecnomatix 2307 Robot Controllers or Tecnomatix 2402 Robot Controllers

Download the file(s):

Tecnomatix_16.1_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_16.1.1_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_16.1.2_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_17.0_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_2206_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_2301_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_2307_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

Tecnomatix_2402_YASKAWA_INFORM_64BIT_v6.58_16_07_2024.exe

To Install:

Place Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8801454

Contents

SummaryDetails

Associated Components