Error loading libmfgammaterialisebp.dll when using the Additive Manufacturing application

2021-10-06T23:27:58Z

Summary


Details

When using the Additive Manufacturing application, some errors appear in the NX log file:

+++ Cannot load image D:\apps\Siemens\NX1953\NXBIN\libmfgammaterialisebp.dll

+++ Cannot load library libmfgammaterialisebp

+++ Requested library could not be loaded.

What is the problem and how can this be avoided?

Solution

Make sure that the build processor interface has been installed, according to the documentation:
https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200507135732916.xid1415830/html/xid1410539

After doing that, the errors should not appear anymore.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ADD_FIXED_PLANE
Version: V1953
Function: BUILD_PROCESSOR

Ref: 002-8547635

KB Article ID# PL8547635

Contents

SummaryDetails

Associated Components