Solid Edge Clear existing entries from Dimension Prefix pull-down list

2021-10-06T23:58:38Z
DRAFT

Summary


Details

Is it possible to clear the existing entries in the Dimension Prefix pull-down list?

 

Solution

Currently it is not possible to clear the existing entries from the Dimension Dialogs pull-downs e,g, Prefix from inside Solid Edge.

Solid Edge stores this entries in the Windows Registry in the HKEY_Current_USER registry hive of the currently logged in user.

With care, use the Windows Registry Editor (Microsoft Start > Button > type regedit > select the listed Registry Editor) to remove the appropriate entries from the Solid Edge Dimension registry key hive.

Registry Hive:

Computer\HKEY_CURRENT_USER\Software\Siemens\Solid Edge\Version xx\PrefSets\Dimension

Go to the registry hive and remove the Prefix Strings. 



Notes and References

Note: Use this same workflow for the other dimension pull-down fields e.g. Suffix

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V221MP4
Function: DIMENSIONS

Ref: 002-8547228

KB Article ID# PL8547228

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS