Simcenter 3D Solutions How Force boundary condition works for tet and hex mesh?

2021-10-06T23:27:58Z
Simcenter 3D

Summary


Details

How Force boundary condition works for tet and hex mesh?

Solution

The force on a surface is distributed to the underlying mesh in a manner that yields a uniform pressure across the mesh. The forces are distributed to the nodes using the element shape functions.

The linear shape functions distribute that in a manner that results in each node on that face getting an equal percentage of that faces load (1/3 for trias, 1/4 for quads). With parabolic shape functions, the forces end up being 0 at the corner nodes so you only see values on the midnodes.

This is the standard one  used across all commercial FEA codes


Notes

KB Article ID# PL8547205

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow