Support information for the color of convergent body/face in CATIA V5 translator
2021-10-06T23:27:58Z
Summary
Details
Now Convergent body in NX can be exported to Point cloud mesh in CATIA V5, but the color does not export by CATIAV5 translator.
Step to reproduce: 1. Create a convergent body in NX 2. File > Export > CATIA V5 3. Open the part in CATIA V5
*** no any color exports.
Solution
Export translation of the color for convergent body is not currently supported. This is a technical limitation imposed by cloud of points. Only Face/Line/Curve color have been supported. You can see the supported information in the documentation.
However, the information about Point cloud mesh has not been clearly stated in the documentation and is difficult to understand, so it will be explicitly stated in NX1980 release notes.