Faces cannot be selected when creating holes

2021-10-06T23:27:58Z

Summary


Details

New enhancement  "Simplified point selection" for Hole command has been released in NX1953, but I can't select an input face if I try to create a new hole.

Step to reproduce: 


1. start nx > open a new part


2. Create a box, some holes like below > save the part

3. Customer Default > Modeling > General > Miscellaneous > Turn off "Automatically Sketch on Planar Faces".


4. restart NX and open the part


5. double click "Hole" feature in PNT for editing > push "Cancel" button or add a hole.


6. Please try to put new Hole in a face.



*** cannot select any faces at all.

Solution

Work around:


1. By making use of "Sketch Section" option, specify the locations with launching Sketch environment.

or


2. Restart NX and create new hole

Notes and References

The condition to reproduce the issue is:


    Turn off "Automatically Sketch on Planar Faces". Therefore, in case of turning on the setting is not happened the issue.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1961
Function: FEATURE_MODEL

Ref: 002-8545835

KB Article ID# PL8545835

Contents

SummaryDetails

Associated Components