Fonts for single point engraving are not seen in the drop down list when creating a "Note" from the Manufacturing Ribbon.
Review the problem- Go to the Geometry group on the Ribbon.
- Select the drop down as seen in the image below.
None of the NX fonts appeared in the available fonts.
Solution
- Go to Customer Defaults.
- Selecting Drafting--General/Setup--Miscellaneous tab--Fonts to Use.
- Select Standard and NX Fonts.
Please see image below.

- Select OK on the dialog box and restart "NX".
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1969
Function: PLANAR_MILLING
Ref: 002-8544935