The mass of an assembly or sub assembly is not correct updated and shows "0".
Solution
The quantity value of component is zero, so that the mass properties is zero.
To get the corresponding result, editing the quantity from
0 to
1 needed.
Please notice the Screenshots for the steps:

Step 1:
Select the sub assembly and change Quantity from
0 to
1

Step 2:
Recalculate the mass by "update the Mass Properties now"!
The Mass calculation should now show the correct Mass.

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1965
Function: WEIGHT_MANAGE
Ref: 002-8544787