Solid Edge Unable to edit Synchronous dimensions simultaneously

2021-10-06T23:58:35Z
PART/SHEETMETAL

Summary


Details

I create a sketch in Synchronous mode and select multiple dimensions using Ctrl+ Select and define a value.  The dimension that was selected first is updated to the modified value - the other dimension does not.

This issue appears to occur in Solid Edge 2021 but not in Solid Edge 2020.  Why?

Solution

When the Auto-Scale Sketch option is ON you can edit only one driving dimension.  To enable editing of multiple dimensions you will need to turn the Auto-Scale Sketch option OFF. 

This option is OFF by default in Solid Edge 2020 but is ON by default in Solid Edge 2021 - which is why we implemented the pop-up informing users about this option.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V221.0
Function: SYNCSKETCH

Ref: 002-8544724

KB Article ID# PL8544724

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES