How to reduce intermediate Rotary moves in Multiaxes NC Output.

2021-10-06T23:27:57Z

Summary


Details

Need to combine consecutive rotary moves (rapid move motion 
type) into a single move when there is no change in X, Y and Z. 
For E.g: 
N1 G0 G53 Z0. 
N2 T01 M6 
N3 G54 
N4 G17 G0 G90 X0. Y45.347 A-90. C0. S2000 M3 
N5 G43 Z85.347 H1 
N6 G94 G81 G98 Z28.944 F200. R48.214 
N7 G80 
N8 G0 X0. Y45.347 Z85.347 C2.647 
N9 C5.294 
N10 C7.941 
N11 C10.588 
N12 C13.235 
N13 C15.882 
N14 C18.529 
N15 C21.176 
N16 C23.824 
N17 C26.471 
N18 C29.118 
N19 C31.765 
N20 C34.412 
N21 C37.059 
N22 C39.706 
N23 C42.353 
N24 C45. 
N25 G81 Z28.944 F200. R48.214


Need C45 directly instead of intermittent C outputs. 



Solution

The best way to satisfy this requirement will be to use a preconfigured layer in the post configurator. 
Layer name: Combine Rotary layer. 
This combine rotary layer enable the users to combine consecutive rotary moves (rapid move motion 
type) into a single move when there is no change in X, Y and Z. The layer includes tcl and psl files. Post 
writer can import this layer by PC layer manager to any machining postprocessors. 
This layer only works for NX1899 and later versions. 

This layer is available in Posthub site: 
https://posthub.sws.siemens.com/#/kits 
Search for Layer in the Search dialogue box and you will find the Combine Rotary layer. 
The folder contains documentation on how to apply the layer and the use case. 

You can refer to this site for information on Layers:


https://docs.plm.automation.siemens.com/tdoc/nx/1899/nx_help#uid:xid1128418:index_m 
fgpostconfig:xid1487919:xid1446295 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V9.0.3
Function: POSTCONFIG

Ref: 001-10009880

KB Article ID# PL8544603

Contents

SummaryDetails

Associated Components