Issue:
When migrating parts from I-deas to NX, part materials will have wrong values in NX.
i.e: The material properties from Ideas are migrating with units of density as kg/m^3 instead of kg/mm^3. The expression should look correct but the computed value is incorrect.
The migration of the part should complete normally and generate an NX part that is valid for further migration of parent assemblies and drawings.
Solution:
A patch for NX 1899, NX 1926 and NX 1953 has been posted to Solution Center under Content Migration Manager for I-deas - I-deas Material Patch.
Please follow the instructions in Readme.txt to install the patch.
SFB-NX-8544027
Product Information:
- Product: NX , Application: CMM