What is the difference between the Agent Modules in Package Builder?
Solution
There are two Agent modules available for customization in Package Builder, the Basic Agent and the standard Agent module.
The Basic Agent is designed for motion controlled low voltage motors. Its functionality is limited and meant solely for onboarding and authentication. Ingesting any additional data with this module is not possible.
The standard Agent Module is designed to collect and transmit multiple data points to MindSphere from devices or applications for monitoring and analysis.
Unless there is a specific use case for the Basic Agent, the standard Agent Module should be used when ingesting data to MindSphere is required.
Notes