Older version of Internal Sketch cannot be edited/renewed

2021-10-06T23:27:57Z

Summary


Details

Internal sketches created in nx1926 or before are not renewed and converted to new sketch and it is not possible to edit them any longer.




Step to reproduce: 


1. In NX1926 Series or before, open a new part and create some body > Pattern Feature, Mirror Feature or etc > Save the part.


    - Make sure to create the body with Internal Sketch in Extrude or etc.



Case 1: Pattern Feature and Extrude Feature which has Internal Sketch:

KB Article ID# PL8542670

Contents

SummaryDetails

Associated Components