How to control the reference sets when generating MONOLITHIC JT from NX Assembly?

2021-10-06T23:27:57Z

Summary


Details

How to control the reference sets when generating MONOLITHIC JT from NX Assembly?



Solution

The said Requirement is possible using the load options file. 


Consider an example of an Assembly like mentioned below -


An assembly has 3 parts, and each part contains BLOCK, CYLINDER, and SPHERE reference sets along with these geometries. Assembly is configured with BLOCK Reference Set of Part1, CYLINDER Reference Set of Part2, and SPHERE Reference Set of Part3. Refer to the below snapshot for more details on the Assembly structure –

Now I want a monolithic JT with only the BLOCK Reference Set of each part. So, I specified the "BLOCK" reference set in the load_options.def file. Refer to the below syntax of Load option File –

LoadOptions_ReferenceSets: "BLOCK" "As Saved" "Use Model" "Entire Part" "Empty"


*****************************


LoadOptions_SearchPaths: "C:\\Program Files\\Siemens\\NX1202\\UGII..." 


LoadOptions_LoadComponents: load_all_components


LoadOptions_PartLoadOption: partially_load


LoadOptions_LoadWAVE: NO


LoadOptions_LoadWAVEParents: NONE


LoadOptions_LoadSubstitution: dont_allow_substitution


LoadOptions_LoadLatest: NO


LoadOptions_LoadOption: load_from_dir


LoadOptions_ManagedModeLoadOption: load_by_revision_rule


LoadOptions_LoadFilters: load_no_components


LoadOptions_LoadFailOption: dont_abort


LoadOptions_ReferenceSets: "BLOCK" "As Saved" "Use Model" "Entire Part" "Empty" 


LoadOptions_ApplyAllLevels: NO


LoadOptions_GenerateMissingPFM: YES


LoadOptions_BookmarkRefSets: Import


LoadOptions_BookmarkPartsLoad: Load_Visible


LoadOptions_BookmarkRestoreFullyLoadedState: no


LoadOptions_SubsetLoadBehavior: Do_Not_Update


*****************************


Now specify the load option file on the command line using the UGII_LOAD_OPTIONS variable as shown below and then provided the translator command.

So, after translation to Monolithic JT below is the results output with Block Reference Set geometries only-



Notes and References

9922673 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: TRANSLATOR
Version: V1946.4000
Function: NX_JT

Ref: 002-8541492

KB Article ID# PL8541492

Contents

SummaryDetails

Associated Components