Solid Edge Is there a way to batch convert Solid Edge documents to neutral format such as STEP?

2024-09-19T15:53:27Z
TRANSLATORS

Summary


Details

Is there a way to batch convert Solid Edge documents to neutral format such as STEP?

Solution

You can use the sample VB program 'Custom/Batch/bin/Batch.exe' which is delivered in the Solid Edge installation folder. For Version 2021 or newer, you will need to go to Support Center where you downloaded Solid Edge. In the "Solid Edge 2021 Add-ons" section, you will find "Solid_Edge_Sample_Programs_2021.zip" which contains the same sample programs which were delivered with earlier versions.

Notes

For more Solid Edge STEP related articles, please refer to the "Solid Edge STEP FAQs Collection"

KB Article ID# PL8540269

Contents

SummaryDetails

Associated Components

TRANSLATORS: OTHER