How to control the JT File size while exporting from NXtoJT?

2021-10-06T23:27:57Z

Summary


Details

How to control the JT File size while exporting from NXtoJT? 



Solution

In an ideal condition when you have the settings of tessUG.config file as shown below: 

LOD "1" { 
 Level = 1 
 Chordal = 0.001 
 Angular = 20 
 Length = 0 
 AdvCompressionLevel = 0 

Here, Angular=20 means you get 360/20 chords details per full circular shape. 
 
Avoid using the "0" value for Angular in LOD "1".


Please note to arrive at an optimal value, we need to use the trial and error method. 
You may want to increase the Angular value to say 25, 30, or even more and verify the size and shape of the files generated for its acceptability. Also, ensure to play around with Chordal value to get better results.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1909
Product: NX
Application: TRANSLATOR
Version: V12.0.1
Function: NX_JT

Ref: 001-10055143

KB Article ID# PL8540265

Contents

SummaryDetails

Associated Components