Interaction method does not work on dialog memory in Displayed Properties dialog
2021-10-06T23:27:57Z
Summary
Details
Part file saved with interaction method "Bulk" in Displayed part properties, when opened in NX1953, it shows interaction method as "Traditional" and it shows as "Bulk" when opened in NX1863.
Solution
The behavior has been changed from NX1872 onwards.
For single part selection, the default Interaction method will be "Traditional" in the Displayed Properties dialog, since this is the preferred edit mode for single part attributes. Whereas for multiple Part selections, the default Interaction method will be "Bulk" which is the preferred edit mode for multiple part attributes.
Hardware/Software Configuration
Platform: INTEL OS: windows OS Version: 1064 Product: NX Application: ARCHITECTURE Version: V1953 Function: USER_ATTRIBUTES