Easy way to Identify Driving and Driven Dimension when the sketch is inactive.

2021-10-06T23:27:56Z

Summary


Details


Easy way to Identify Driving and Driven Dimension when the sketch is inactive.

Solution


Currently, we are using the method active sketch and refer "edit" dimension dialog box to Identify Driving and Driven dimensions.


Now, we can Identify dimensions in the graphical Window itself by select dimensions and look at the Dependencies Pane without using the sketch active and edit dimension.


It reduces time to identify the Driving and Driven dimensions.


NOTE: If driven it displayed as "Linear Dimension"

Once identify the dimension we can change the dimension color to Identify it in the graphical window by
Object Display,

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1953
Function: DRAWING/VIEW

Ref: 002-8533210

KB Article ID# PL8533210

Contents

SummaryDetails

Associated Components