Map Teamcenter workflow Signoff data to Solid Edge draft

2021-10-06T23:58:29Z

Summary


Details

The customer wants to have the Teamcenter workflow signoff values on their Solid Edge draft. The Solid Edge draft is processed by a simple workflow that will release the Item Revision and the associated SE part and SE draft dataset:
What attribute mapping should be used to get the status, approver and release date on the SE draft?



Solution

First of all: the used workflow must have a signoff task! This will not work with a Quick- or TCM- Release workflow.

Example Workflow:

Attribute mapping:


{ Dataset type="SE Draft"
                {Item type="Item"
                               "TCMapStatus" : ItemRevision.release_status_list.name /master=iman /description="Release Status"
                               "Signoffdesigner" : ItemRevision.Job.SIGNOFF(Designer).group_member.user.user_id /master=iman /description="Signoff Designer"
                               "Signoffdate" : ItemRevision.Job.SIGNOFF(Designer).decision_date /master=iman /description="Signoff Date"          
                }
}

If you open the SE draft after the release workflow you will see the signoff date in the file properties:

You can add the signoff data with property text to the Solid Edge template:


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 002-8531168

KB Article ID# PL8531168

Contents

SummaryDetails

Associated Components