When opening a part which "Mirror Display" command is executed and saved, the "Mirror DIsplay" toggle button is not turned on even though the model data in graphic window is actually mirrored and shown correctly.
*** It seems to happen the issue in case of opening the part first time after starting NX.
Step to reproduce:
1. Open a part and create any body like below.
2. Go to "Analysis" tab > toggle "Mirror Display" on. 3. Save the part > restart NX > go to "Analysis" tab and then look at the toggle button.
Work around: Toggle "Mirror Display" on explicitly.
Solution
It's fixed in NX2007.
Notes and References
After applying the WA above, no issue occurs anymore if closing the part without saving and reopening it during the same session.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: STUDIO_DESIGN Version: V1926 Function: ANALYZE