NX Explanation of Syslog on Failure to populate or load drafting standard data in level "x"

2021-10-06T23:27:56Z
NX for Design

Summary


Details

The NX syslog shows information about drafting standard data in levels: 

 Failed to populate drafting standard data in level 1. 
 Failed to populate drafting standard data in level 2. 
 Failed to populate drafting standard data in level 3. 
 Unable to load drafting standard (null) at the 1 level 
 Unable to load drafting standard (null) at the 2 level 
 Unable to load drafting standard (null) at the 3 level 
Processing drafting standard file 
 Unable to load drafting standard (null) at the 4 level 


Question: 
What are the meaning of these level? 



Solution

Below is the "mapping code" for the level number that shows up in the syslog:


0 - Shipped 
1 - Package 
2 - Site 
3 - Group 
4 - User 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V1847
Function: CUSTOMER_DEFS

Ref: 001-10040080

KB Article ID# PL8530844

Contents

SummaryDetails

Associated Components

Modeling