NX
Setting "No Selection Filter" as the default selection filter in Manufacturing
2021-10-06T23:27:56Z
NX for Manufacturing
Summary
Details
Since NX 1899 the default selection filter (Type Filter) option is set to "Tool Path" when entering Manufacturing.
Is it possible to change back to the previous default option of "No Selection Filter"?
Solution
From NX 1926 there is a setting to control this behaviour in the Customer Defaults. It can be found under "Manufacturing --> Tool Path Display --> General --> Path Display and Selection --> Select Tool Path". If that option is toggled off, the default selection filter will be "No Selection Filter".
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: CAM Version: V1926 Function: USER_INTERFACE