Solid Edge Cannot select font in Text Profile command

2021-10-06T23:58:27Z
PART/SHEETMETAL

Summary


Details

When using a custom font, the font is usable within Windows and other applications but the font is not shown/not selectable/missing within the Solid Edge Text Profile command.  Why?


Solution

Currently the Text Profile command supports TrueType fonts or .ttf files only.

If the font is not a TrueType font e.g. OpenType (.otf) font then the font will not be selectable within the Text Profile command.


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V221.0
Function: GEOMETRY

Ref: 002-8530802

KB Article ID# PL8530802

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES