Constraints are disappearing in the new Sketcher

2021-10-06T23:27:56Z

Summary


Details

Relations (constraints) that are manually added in the new Sketcher do not stay, and can disappear when adding more dimensions. 



Solution

In the new Sketch, relations (formally known as constraints) are not meant to be permanent. They simply move the curves into place. The manually added relation is not enforced. As a workaround, try turning on 'Create Persistent Relations', then manually create the relation/constraint. This will help the new relation "stick". 
Please note that 'Create Persistent Relations' is not on by default and may be hidden. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1953
Function: SKETCHER

Ref: 001-10038922

KB Article ID# PL8530725

Contents

SummaryDetails

Associated Components