Details
Opening a .SAT File (ACIS file type) with Solid Edge 2021 will fail and the log file reports:
Error!No entities to translate
Solution
This is a known behavior with Solid Edge 2021 and will be resolved in the upcoming Solid Edge version 2022.
As a workaround for Solid Edge 2021 it is possible to open the SAT file if the file extension is changed from uppercase ".SAT" to lowercase ".sat".
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V221MP4
Function: ACIS-SAT
Ref: 002-8530391