NX
PMI compare is not working in NX1926, 1930, 1934 or 1938.
2021-10-06T23:27:56Z
NX for Design
Summary
Details
We are not able to compare the PMIs between 2-parts. After launching the PMI compare dialog, select the source & target part and clicking OK, no information or visual report generated.
Steps to reproduce: 1.Prepare for 2 sample models. (something such as one box solid with one PMI.) 2.Start NX > go to PMI environment. 3.Launch PMI Compare function > select Loaded and Comparison Parts each other > OK.
The function does not work at all.
Solution
It was fixed in NX1942 and NX1953 Series.
No WA exists in NX1926, 1930, 1934 or 1938 unless MBD license is included in your license file.
Notes and References
PMI Compare functionality must be in production with PMI license, but the cause of the trouble was due to in production with MBD license. The issue always occurs under a condition which doesn't have MDB license.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: PMI Version: V1934 Function: ADVISOR