Solid Edge 2D Nesting is not nesting sheetmetal part.

2021-10-06T23:58:23Z
PART/SHEETMETAL

Summary


Details

2D Nesting will not nest a sheetmetal file.



Solution

This can happen if the Layer/Color assignment options that are located in the lower left window pane are not selected. This must be set to cut so that the boundaries can be created.

Note: Flat patterns must also exist in a sheetmetal file in order for the parts to be nested. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V221.0
Function: FILE

Ref: 001-10028996

KB Article ID# PL8530005

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN