Changing the default settings for CLSF output file names.

2021-10-06T23:27:56Z

Summary


Details

How to change the default settings for CLSF output file name as operation name.

Solution

Please find the below steps to change the clsf file name to operation name

1) Set the environment variable "UGII_CAM_SETUP_ROOT_DIR = D:\Sample folder" (This is for example).


2) Open NX and go to Manufacturing 


3) On Menu -> Preferences -> Manufacturing -> Change the configuration file to "cam_library.dat


 4) Now if we select the Program name then it outputs program group name and if we select the operation it outputs the operation name.


 
The  output files will be in the " D:\Sample folder_partname" specified in the above environment variables.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1953
Function: CLSF

Ref: 002-8529962

KB Article ID# PL8529962

Contents

SummaryDetails

Associated Components