Solid Edge Would like Save As to exclude draft files.

2021-10-06T23:58:23Z
DOC_MANAGEMENT

Summary


Details

When doing a Save As on models managed by Teamcenter/SEEC is there a way to save only the models and not the draft files? Currently a Save As saves all the draft files in the item revision. 



Solution

There is an "Exclude Draft" command that can be used to exclude the draft files when doing a Save As on models. In the Model environment go to the Teamcenter tab. The "Exclude Draft" toggle is directly to the right of the Save As command. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 001-9807898

KB Article ID# PL8529872

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC