"No Drawing Found" error is returned when Open Drawing command is selected

2021-10-06T23:58:22Z

Summary


Details

While working in a Solid Edge Data managed model file, the user selects the "Open Drawing" command from the toolbar.  The expectation is that a Solid Edge Draft file will be opened that contains drawing views of the currently opened model file.  Instead, the user is returned the following error message: "No Drawing Found", even though a drawing does exist in the vault.

Solution

This error message will occurring if the Vault location is not defined in the Solid Edge Options -> Manage -> Vault Definitions page.  This location must be defined correctly in order for the Windows Search Index to be accessed from the Solid Edge client.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEDM

Ref: 002-8529870

KB Article ID# PL8529870

Contents

SummaryDetails

Associated Components