Importing non-Solid Edge document (PDF) into Teamcenter

2021-10-06T23:58:22Z

Summary


Details

Importing non-Solid Edge document (PDF) into Teamcenter 

Solution


Importing non SE documents is not possible and not supported with ATT.

So it's not possible to import Standalone non SE document (PDF) to TC using ATT.

Only those non SE documents which have link with SE data can be imported to TC.

Below is the example for non SE document which can be imported to TC.

Excel file can be imported to TC using ATT if that has relation with SE data( Se part/asm created using variable table).


 



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP13
Function: SEEC

Ref: 002-8529865

KB Article ID# PL8529865

Contents

SummaryDetails

Associated Components