NX Dependency between upward face chosen and inferred bending directions in flat pattern view

2021-10-06T23:27:56Z
NX for Design

Summary


Details

Can you enlighten upon the dependency between upward face chosen to create flat pattern view and bending directions that are inferred?



Solution

Upward face is an user input.


If the included angle between two adjacent upward faces are within 180 degrees, then the bend direction is "UP"  else it is "DOWN"



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: FLAT_PATT_VIEW

Ref: 002-8529854

KB Article ID# PL8529854

Contents

SummaryDetails

Associated Components

Drafting