PMI hole callout dimension can't be added to a patterned hole

2021-10-06T23:27:55Z

Summary


Details

1. Create a block and add threaded hole feature


2. Create pattern feature (i.e. linear pattern 2x2)


3. Try to add PMI hole callout dimension


 
Only base feature is selectable not the remaining patterned 3 features.


In 1867 all were selectable.



Solution

The default value in Pattern Feature dialog is changed in the latest versions. That's why you see the difference.


Change the pattern method to "Variational" in Pattern Feature dialog for getting each instances selected



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: PMI
Version: V1934
Function: DIMENSION

Ref: 002-8529845

KB Article ID# PL8529845

Contents

SummaryDetails

Associated Components