NX cannot be switched to routing application with "Routing: Application view cannot be loaded" error.
The log file reports the below error.
*** EXCEPTION: Error code 1525041 in line 4622 of
+++ Failed to parse application view, parser error : UGXML Error at file C:\APP\NX1926\routing\ugroute_elec\appview\ugroute_elec_metric.xml : line 108, column 22
element 'Bend_Radius_Table_Files' is not allowed for content model '
Solution
Bend radius table settings mentioned in your "ugroute_elec_metric.xml" is not supported in the latest versions.
You need to remove the below texts from your xml file.
<Bend_Radius_Table_Files>
<!--
<File_Name>
pipe_bend_radius_table.txt
</File_Name>
<File_Name>
tube_bend_radius_table.txt
</File_Name>
-->
</Bend_Radius_Table_Files>
In addition, texts files also not supported, you need to use a spreadsheet file (*.xlsx)
In the latest versions, if you would like to use bend radius , you can set up the location of the bend table from below customer defaults.

Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ROUTING_GENERAL
Version: V1926
Function: REUSE_LIBRARY
Ref: 002-8529842