Details
Just like the behaviour of shipped Gear(or Pump) symbol of logical routing, I would like to add automatic labelling on customized library parts.
How to add automatic labelling of Reference ID in the custom library parts?
Solution
Logical Routing places a label automatically after a symbol is placed, with the text of the note being populated by the value of the characteristic REFERENCE_ID assigned to the occurrence of the symbol part.
The symbol is required to contain a point named NOTE_ORIGIN and a point named LEADER_ORIGIN. If either of these points do not exist, or the symbol does not have the characteristic REFERENCE_ID , then a note is not placed
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ROUTING_LOGICAL
Version: V1919
Function: TOOLS
Ref: 002-8529841