How to control maximum value for an expression in NX?

2021-10-06T23:27:55Z

Summary


Details

How to control maximum value for an expression in NX?


For e.g. 


 There is an expression X = 25mm. 


And I would like to predefine the maximum value that users can set for X is 30mm.


How can I set that?



Solution

For this case, the user can add a check to validate the values of expressions.


The steps:


  1. Right click on expression X in Expressions dialog->Add a check
  2. Click New Requirement
  3. Enter any name for the requirement
  4. Select "Definition Method" to "Single Sided Comparison"
  5. Set <= 30
  6. Now if the user enters any value greater than 30, it will be indicated as 'Check Result= Failed"  in Expression dialog



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1953
Function: EXPRESSION

Ref: 002-8529839

KB Article ID# PL8529839

Contents

SummaryDetails

Associated Components