Facet Bodies can only be used with tolerant machining

2021-10-06T23:27:55Z

Summary


Details

Operation: Cavity Mill

Subtype: Undercutting        Tool: T-cutter

In order to allow undercutting in the operation, Tolerant machining needs to be Turned Off. 
But, While generating this toolpath the following warning is received.

"Facet Bodies can only be used with tolerant machining"

Solution

The solution is to use a modeled solid body instead of bounding box as a blank in the Workpiece Dialog.


  1. If the Blank is selected as a Solid Body in workpiece => toolpath will be generated.
     2.If the Blank is selected as a Bounding Box in workpiece => Facet Body is created internally => error                 message as per rule.






Notes and References






Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1953
Function: CAVITY_MILLING

Ref: 002-8529830

KB Article ID# PL8529830

Contents

SummaryDetails

Associated Components