Angular Dimension Round-Off not working to specified number of decimals.

2021-10-06T23:58:21Z

Summary


Details

Why is dimension Round-Off not working to the specified number of decimals? 



Solution

Trailing zeros are not on. Go to Styles, Dimension, select the style you are using and click modify. Go to the Units tab and turn trailing zeros. You can also set the roundoff here if you need to change it in this file.

These settings are stored in the file, so if this is something that will always or almost always be used, we recommend setting this in your Draft template file



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V221.0
Function: DIMENSIONS

Ref: 001-10028671

KB Article ID# PL8529746

Contents

SummaryDetails

Associated Components