"JT plus PDF" not support for attribute displayed as part name in Assembly tree.
2021-10-06T23:27:55Z
Summary
Details
I exported TDP with "JT Plus PDF method" and opened the exported PDF in TCVis( or JTtoGO), but the JT data in "Model Workspace" and the component node in "Project Workspace" are not highlighted even though selecting the component from the "BOM Table" list.
Steps to reproduce: 1. Prepare for the template like below. Make sure to use "Attribute" as the appeared name field instead of "Part Name". - Set "Attribute" as "Column" like below and save the template. 2. Open a new part and create a simple assembly like below. 3. Assign one property to the top assembly like below. PART_NO="AAAAAA" 4. Change Assembly Preferences such as below Miscellaneous -> "Specified Attribute" Attribute - > "PART_NO" 5. PMI > Publish - Select "JT plus PDF" as the method - Select the template to be created in Step 1 above.
Solution
Currently, "Specified Attribute" has not been supported by the function. Please use "File Name".
Notes and References
The matrix on Highlight/No Highlight behavior between the setting of Assembly Preference and TDP Template when clicking a node in BOM table is as follows.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: TECH_DATA_PKG Version: V1953 Function: PUBLISH