Exporting multiple sheets of NX Assembly file to AutoCAD 'modeling' Not 'Layout'
2021-10-06T23:27:55Z
Summary
Details
I want to export multiple sheets of an NX part or Assembly to AutoCAD 'modeling'. Currently NX allows to select multiple sheets only when the export to 'Layout' option is selected.
Steps to reproduce: 1. Open a new part > create a simple body like a box solid. 2. Go to Drafting > create multiple drawings. 3. File > Export > AutoCAD DXF/DWG... - Select "Modeling" as "Output to" - Change to "Drawing" for "Data to Export". After that, please try to select multiple drawings. It's not possible to select multiple.
Solution
The capability is implemented in NX1980 Series. - You can now select multiple drawings at a time and export them to Autocad "modeling". - As the result, 2 dxf files export as below.
For NX1953 or before, WA is to output the sheets one by one.
Notes and References
The behavior was design limitation and the function was not supported until NX1953 Series.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: TRANSLATOR Version: V12.0.2 Function: DXF_DWG