How to create a cylindrical dimension that is bent at a right angle.

2021-10-06T23:27:55Z

Summary


Details


 How to create a cylindrical dimension that is bent at a right angle.


 


Solution



1. Drafting Application.


2.Menu>Insert>Dimension>Linear.


3.Create a Cylindrical Dimension using centerline and edge.




4.Edit as Single Sided dimension.



5. Set Orientation and Position

Orientation: Text at Specified Angle.
Angle : 0 [zero degree]
Position: Text above Stub.



5.Create a cylindrical Dimension at a right angle and it will be placed as shown below.



 


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1953
Function: DIMENSION

Ref: 002-8529618

KB Article ID# PL8529618

Contents

SummaryDetails

Associated Components