Solid Edge Not able to open NX 1926 part file in Solid Edge 2020 in manage mode.

2021-10-06T23:58:20Z
DOC_MANAGEMENT

Summary


Details

Not able to open NX 1926 part file in Solid Edge 2020 in manage mode. 

Solution

NX 1926 is not supported with SE2020.


Below is the supporting matrix.


SE2020MP5 - NX1899
SE2021RTM - NX1899
SE2021MP1 - NX1926


So to overcome this need to downgrade NX to NX1899 with which NX part file can be opened in SE 2020 MP5 or need to upgrade SE to SE2021 Mp1 to open NX 1926 part file.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 002-8529602

KB Article ID# PL8529602

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC