Can the detached origins of a hole table be re-attached?

2021-10-06T23:58:19Z

Summary


Details

Can detached hole table origins be re-attached? 



Solution

Yes. 
In the Dimensions Group, go to the Attach Dimension command. 
Select the X1 origin dimension line, then select the edge you want to attach it to. 
Do the same thing for the Y1 origin dimension and edge. 
The origin dimension will now be attached.


Update the view and you will see that the Hole Table updates as well. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V221MP4
Function: DIMENSIONS

Ref: 001-10025259

KB Article ID# PL8529409

Contents

SummaryDetails

Associated Components